Help for Interfacing HC-SR04 Ultrasonic Sensor with LPC 1115 Rev A Eval Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help for Interfacing HC-SR04 Ultrasonic Sensor with LPC 1115 Rev A Eval Board

2,461 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rvalvekar on Sun Aug 31 08:15:06 MST 2014
Dear and Respected,

I am trying to interface HC-SR04 Ultrasonic Sensor with LPC 1115 Eval Board. I am stuck with the timer controls for LPC 1115. Could i get some help with the Timers and Controlling those with respect to HC-SR04?

Thank You

Rohan Valvekar
Labels (1)
0 Kudos
Reply
2 Replies

2,237 Views
anilkumarraj200
Contributor I

Hi,

Can anybody can share the logic for calculating the pulse using time32 on lpc11u4x platform.

regards

0 Kudos
Reply

2,237 Views
soledad
NXP Employee
NXP Employee

Hi,

I suggest to check the following application note:

https://www.nxp.com/docs/en/application-note/AN11538.zip 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply