Hard fault Handle error LPC54606 Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hard fault Handle error LPC54606 Microcontroller

30,450 Views
vijay_123
Contributor I

I Run the sample code of USB_CDC_VCOM_BM. In IAR Showing Hard fault Handle error and Accessing Illegal memory address, When Debugging the code. Kindly If anyone find the solution let me know

/*! @brief FROHF clock setting API address in ROM. */
#define CLOCK_FROHF_SETTING_API_ROM_ADDRESS (0x030091DFU)

/*showing Hard fault error when reach this function*/

#define set_fro_frequency(iFreq) (*((void (*)(uint32_t iFreq))(CLOCK_FROHF_SETTING_API_ROM_ADDRESS)))(iFreq)

i'm not sure, why its showing error, SO I attached Example code

##SDK version - 2.13.0

Using ##Lpc54606j256 microcontroller, IAR TOO

0 Kudos
Reply
14 Replies

30,379 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding your question of hard-fault error when the code is executed.

Pls check the following items:

1)disable interrupt before you call the api function, after calling, enable interrupt.

__STATIC_FORCEINLINE void __enable_irq(void)
{
__ASM volatile ("cpsie i" : : : "memory");
}

 

__disable_irq();

set_fro_frequency(96000000);

__enable_irq();

 

 

xiangjun_rong_0-1696817653773.png

2)enable ROM bit in SYSCON->AHBCLKCTRL0|=1<<1; in this way, you can call the ROM code

3)Because set_fro_frequency(96000000); function configure the FRO to output 96MHz clock, it is unnecessary to configure the SYSCON->FROCTROL in application code.

 

Pls have a try

BR

XiangJun Rong

 

30,359 Views
vijay_123
Contributor I

Hi XiangJun Rong,
Thank you for your reply.
Again, Same Error and same line but I Changed code as per your suggestion.

0 Kudos
Reply

30,350 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls try to use the SDK example to set the 96MHz clock as main clock

void BOARD_BootClockFROHF96M(void)
{
/*!< Set up the clock sources */
/*!< Set up FRO */
POWER_DisablePD(kPDRUNCFG_PD_FRO_EN); /*!< Ensure FRO is on */
CLOCK_AttachClk(kFRO12M_to_MAIN_CLK); /*!< Switch to FRO 12MHz first to ensure we can change voltage without accidentally
being below the voltage for current speed */
POWER_SetVoltageForFreq(96000000U); /*!< Set voltage for the one of the fastest clock outputs: System clock output */
CLOCK_SetFLASHAccessCyclesForFreq(96000000U); /*!< Set FLASH wait states for core */

/*!< Need to make sure ROM and OTP has power(PDRUNCFG0[17,29]= 0U)
before calling this API since this API is implemented in ROM code */
CLOCK_SetupFROClocking(96000000U); /*!< Set up high frequency FRO output to selected frequency */

/*!< Set up dividers */
CLOCK_SetClkDiv(kCLOCK_DivAhbClk, 1U, false); /*!< Reset divider counter and set divider to value 1 */

/*!< Set up clock selectors - Attach clocks to the peripheries */
CLOCK_AttachClk(kFRO_HF_to_MAIN_CLK); /*!< Switch MAIN_CLK to FRO_HF */
/* Set SystemCoreClock variable. */
SystemCoreClock = BOARD_BOOTCLOCKFROHF96M_CORE_CLOCK;
}

 

Pls have a try

BR

XiangJun Rong

0 Kudos
Reply

30,345 Views
vijay_123
Contributor I

Hi XiangJun Rong,

In SDK Example, Previously I'm using 96MHz clock as main clock, you can see the Main code for USB, I attached below. 

0 Kudos
Reply

30,320 Views
vijay_123
Contributor I

Hi XiangJun Rong,

Please find the usb example code for your reference, if any changes required let me know

0 Kudos
Reply

30,249 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked your example, it is based on IAR tools, but my IAR tools license  has expired.

I have called the BOARD_BootClockFROHF96M() api function and run it on my LPC54628-EVK board, no problem.

BR

XiangJun Rong

void BOARD_BootClockFROHF96M(void)
{
/*!< Set up the clock sources */
/*!< Set up FRO */
POWER_DisablePD(kPDRUNCFG_PD_FRO_EN); /*!< Ensure FRO is on */
CLOCK_AttachClk(kFRO12M_to_MAIN_CLK); /*!< Switch to FRO 12MHz first to ensure we can change voltage without accidentally
being below the voltage for current speed */
POWER_SetVoltageForFreq(96000000U); /*!< Set voltage for the one of the fastest clock outputs: System clock output */
CLOCK_SetFLASHAccessCyclesForFreq(96000000U); /*!< Set FLASH wait states for core */

/*!< Need to make sure ROM and OTP has power(PDRUNCFG0[17,29]= 0U)
before calling this API since this API is implemented in ROM code */
CLOCK_SetupFROClocking(96000000U); /*!< Set up high frequency FRO output to selected frequency */

/*!< Set up dividers */
CLOCK_SetClkDiv(kCLOCK_DivAhbClk, 1U, false); /*!< Reset divider counter and set divider to value 1 */

/*!< Set up clock selectors - Attach clocks to the peripheries */
CLOCK_AttachClk(kFRO_HF_to_MAIN_CLK); /*!< Switch MAIN_CLK to FRO_HF */
/* Set SystemCoreClock variable. */
SystemCoreClock = BOARD_BOOTCLOCKFROHF96M_CORE_CLOCK;
}

0 Kudos
Reply

30,245 Views
vijay_123
Contributor I

Hi,

I have called the BOARD_BootClockFROHF96M() api function and run it on my LPC54606j256 Microcontroller, but I have problem in this function. Let me know if any other way to find this issue. Past 2weeks working on this still now I didn't solve this issue. So, I need help for this. Please if you have any suggestions tell me and what should i do next?

I'm using IAR Embedded workbench IDE - Arm 9.32.2 tool and SDK version - 2.13.0  

Example - dev_cdc_vcom_bm for USB

I'm also using same BOARD_BootClockFROHF96M(void) function same code, but I don't know, why its not working?

can you tell? should I change tool or SDK version (or) anything changes in my code? 

void BOARD_BootClockFROHF96M(void)
{
/*! < Set up the clock sources */
/*! < Set up FRO */
POWER_DisablePD(kPDRUNCFG_PD_FRO_EN); /*!< Ensure FRO is on */
CLOCK_AttachClk(kFRO12M_to_MAIN_CLK); /*!< Switch to FRO 12MHz first to ensure we can change voltage without
accidentally being below the voltage for current speed */
POWER_SetVoltageForFreq(96000000U); /*!< Set voltage for the one of the fastest clock outputs: System clock output */
CLOCK_SetFLASHAccessCyclesForFreq(96000000U); /*!< Set FLASH wait states for core */

/*! < Need to make sure ROM and OTP has power(PDRUNCFG0[17,29]= 0U)
before calling this API since this API is implemented in ROM code */
CLOCK_SetupFROClocking(96000000U); /*!< Set up high frequency FRO output to selected frequency */

/*! < Set up dividers */
CLOCK_SetClkDiv(kCLOCK_DivAhbClk, 1U, false); /*! < Reset divider counter and set divider to value 1 */

/*! < Set up clock selectors - Attach clocks to the peripheries */
CLOCK_AttachClk(kFRO_HF_to_MAIN_CLK); /*! < Switch MAIN_CLK to FRO_HF */
/* Set SystemCoreClock variable. */
SystemCoreClock = BOARD_BOOTCLOCKFROHF96M_CORE_CLOCK;
}

0 Kudos
Reply

30,221 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls check if the PDRUNCFG0[17,29]= 0U, which power up the ROM.

Pls refer to section 7.5.84 Power Configuration register 0 in UM10912.pdf

/*!< Need to make sure ROM and OTP has power(PDRUNCFG0[17,29]= 0U)
before calling this API since this API is implemented in ROM code */
CLOCK_SetupFROClocking(96000000U); /*!< Set up high frequency FRO output to selected frequency */

BR

XiangJun Rong

0 Kudos
Reply

30,156 Views
vijay_123
Contributor I

Hi XiangJun Rong,

Already, I checked the PDRUNCFG0[17,29] = 0U and Power Configuration register 0, nothing problem in the PDRUNCFG0 register. so, please find the image for your reference. 

0 Kudos
Reply

30,304 Views
vijay_123
Contributor I

Hi XiangJun Rong,

I think problem in ROM Address because Showing error "Memory access error".

/*! @brief FROHF clock setting API address in ROM. */
#define CLOCK_FROHF_SETTING_API_ROM_ADDRESS (0x030091DFU)

/*showing Hard fault error when reach this function*/

#define set_fro_frequency(iFreq) (*((void (*)(uint32_t iFreq))(CLOCK_FROHF_SETTING_API_ROM_ADDRESS)))(iFreq)

0 Kudos
Reply

30,128 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you suspect that the ROM address is incorrect, pls try to execute IAP instruction for example reading part identification number, for detailed inf, pls refer to section 5.6.5 Read part identification number in UM10912.pdf

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

30,016 Views
vijay_123
Contributor I

Hi,

I attached terminal output image for your reference. If I enter something in USB terminal, didn't reflecting in UART terminal because some macros and functions are not defined. so, it's not entering in the functions, I mentioned below and mark in red colour. you can refer the readme pdf for your reference.

#if defined(FSL_FEATURE_USB_KHCI_KEEP_ALIVE_ENABLED) && (FSL_FEATURE_USB_KHCI_KEEP_ALIVE_ENABLED > 0U) && \

defined(USB_DEVICE_CONFIG_KEEP_ALIVE_MODE) && (USB_DEVICE_CONFIG_KEEP_ALIVE_MODE > 0U) && \

defined(FSL_FEATURE_USB_KHCI_USB_RAM) && (FSL_FEATURE_USB_KHCI_USB_RAM > 0U)

if ((s_waitForDataReceive))

{

if (s_comOpen == 1)

{

/* Wait for all the packets been sent during opening the com port. Otherwise these packets may

* wake up the system.

*/

usb_echo("Waiting to enter lowpower ...\r\n");

for (uint32_t i = 0U; i < 16000000U; ++i)

{

__NOP(); /* delay */

}

 

s_comOpen = 0;

}

usb_echo("Enter lowpower\r\n");

BOARD_DbgConsole_Deinit();

USB0->INTEN &= ~USB_INTEN_TOKDNEEN_MASK;

USB_EnterLowpowerMode();

 

s_waitForDataReceive = 0;

USB0->INTEN |= USB_INTEN_TOKDNEEN_MASK;

BOARD_DbgConsole_Init();

usb_echo("Exit lowpower\r\n");

}

#endif

}

0 Kudos
Reply

30,040 Views
vijay_123
Contributor I

Hi,

Now it's working in MCUXpresso IDE, but I don't know why it's not working in IAR. I have problem in MCUXpresso IDE, that problem is some macro definitions and functions are not defined in the code. so, I need your help.

macros:

FSL_FEATURE_USB_KHCI_KEEP_ALIVE_ENABLED

FSL_FEATURE_USB_KHCI_USB_RAM

USB_INTEN_TOKDNEEN_MASK and USB_INTEN_SOFTOKEN_MASK

Functions:

void BOARD_InitHardware(void);

void BOARD_DbgConsole_Deinit(void);

void BOARD_DbgConsole_Init(void);

extern uint8_t USB_EnterLowpowerMode(void);

 

In USB terminal (Tera term) we enter something, it's reflected in UART terminal like printing msg. when we are debugging the code.

We enter something in USB terminal, how do we know USB port data transfer send correctly or not?

I attached code for your reference, can you check and update me.

0 Kudos
Reply

29,949 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you download SDK package based on Windows and MCUXPresso tools.

https://mcuxpresso.nxp.com/en/select

BR

XiangJun Rong

 

0 Kudos
Reply