Flashing and Debugging without using LPC4322 on LPC55S69 using SWD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing and Debugging without using LPC4322 on LPC55S69 using SWD

Jump to solution
3,081 Views
SrinathVelavan
Contributor III

I am developing a custom board design using LPC55S69 as host MCU. In the EVK, the flash programming and debugging is done using LPC4322 as the Link 2 probe with LPC55S69. 

Is it possible to do the flash programming and debugging without using the LPC4322?? Why is the LPC4322 operating at 2.5V on the EVK when it is capable of operating at 3.3V like the LPC55S69?

FYI, I am implementing only the Serial Wire Debug(SWD) interface [ Pins PIO0_11 and PIO0_12]. Is it possible to debug using only the SWD on the LPC55S69? Any information regarding this would be much helpful.

 

TIA

#lpc55s69 #lpc4322

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
3,069 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I review your information and I hope this information could help you.

The proposes of the EVK are only for evaluation and get all in one, and you have a point you do not need to put the LPC43, and that is right, you do not need to add this debugger OB. 

For your new custom board, you will need an external debugger but do not worry this MCU Link JTAG/SWD Debug Probe | NXP Semiconductors is the cheapest debugger from NXP, but there is another option depending on your requirement, Universal Multilink Development Interface | NXP Semiconductors, or J-link Segger all of this support SWD interface.

Let me know if you have doubts.

Best regards,
Pavel

View solution in original post

4 Replies
3,070 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I review your information and I hope this information could help you.

The proposes of the EVK are only for evaluation and get all in one, and you have a point you do not need to put the LPC43, and that is right, you do not need to add this debugger OB. 

For your new custom board, you will need an external debugger but do not worry this MCU Link JTAG/SWD Debug Probe | NXP Semiconductors is the cheapest debugger from NXP, but there is another option depending on your requirement, Universal Multilink Development Interface | NXP Semiconductors, or J-link Segger all of this support SWD interface.

Let me know if you have doubts.

Best regards,
Pavel

3,065 Views
SrinathVelavan
Contributor III

Hi Pavel,

 

Thanks for your immediate response. I am actually implementing the LPC4322 on the board to act as a debugger for LPC55s69. 

I had a followup question:

Why is the LPC4322 operating at 2.5V on the EVK? It is capable of operating at the same voltage as LPC55S69 (3.3V).

Any particular reason or requirement to operate LPC4322 at 2.5v? 

TIA

0 Kudos
Reply
3,046 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I reviewed the Datasheet of this LPC this chart is the voltage of use, I do not about the design of the PCB in specific voltage. 

Pavel_Hernandez_0-1683232523429.png

I recommend review the chapter 10.2 Peripheral power consumption LPC435x/3x/2x/1x Product Data Sheet (nxp.com)

Let me know if you have more doubts.

Best regards,
Pavel

3,035 Views
SrinathVelavan
Contributor III

Thanks for your help. I will look into the peripheral power consumption chapter in the datasheet.

 

0 Kudos
Reply