Hi,
I am Balaji. I am working on LPC 1768 controller. When the controller is in sleep mode, I can't achieve the current reduction specified in the data sheet. I have attached some test results below for your reference. Kindly give me some solution.
Controller | LPC 1768 |
Voltage(RPS) | 3.3 v |
Expected current reduction specified in datasheet | 2mA |
Current reduced when the controller is in sleep mode | Peripherals Enabled |
26mA | GPIO,Timer0 |
25mA | GPIO |
23mA | Timer 0 |
22mA | All Peripherals disabled |
解決済! 解決策の投稿を見る。