Errata sheet LPC546xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errata sheet LPC546xx

1,646 Views
dingelen
Contributor III

I've been going through the errata of this familiy of microcontrollers and found it to have 15 functional problems with the USB and 2 more with the USB_ROM. https://www.nxp.com/docs/en/errata/ES_LPC546XX.pdf

Is it still sensible to use this MCU in a project using USB? Or will this just give me a lot of headaches?

Labels (1)
0 Kudos
Reply
2 Replies

1,549 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tom,

Yes, this Errata is still sensible, we need consider that when programming.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,550 Views
belmontbob59
Contributor IV

One of the  biggest hurdles in my opinion pertains to :

pastedImage_1.png

There is no workaround in the SDK USB stack as far as I am aware of; and I don't see how to implement this from the application side.

0 Kudos
Reply