Errata sheet LPC546xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Errata sheet LPC546xx

1,668件の閲覧回数
dingelen
Contributor III

I've been going through the errata of this familiy of microcontrollers and found it to have 15 functional problems with the USB and 2 more with the USB_ROM. https://www.nxp.com/docs/en/errata/ES_LPC546XX.pdf

Is it still sensible to use this MCU in a project using USB? Or will this just give me a lot of headaches?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,571件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tom,

Yes, this Errata is still sensible, we need consider that when programming.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,572件の閲覧回数
belmontbob59
Contributor IV

One of the  biggest hurdles in my opinion pertains to :

pastedImage_1.png

There is no workaround in the SDK USB stack as far as I am aware of; and I don't see how to implement this from the application side.

0 件の賞賛
返信