EMC and SD/MMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EMC and SD/MMC

1,447件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomkulaga on Wed Dec 19 20:59:51 MST 2012
Is there any practical way of having the EMC and the SD/MMC interfaces on the same chip?

Regards
Tom
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,424件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomkulaga on Sat Dec 29 02:44:16 MST 2012
Thanks for that. I was wondering about the LQFP144 package though, which i don't think its possible.

Thanks anyway.
Tom
0 件の賞賛
返信

1,424件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp21346 on Wed Dec 26 10:53:29 MST 2012
Take a look at the Keil MCB1800/4300 boards. They implement EMC and SD at the same time.

http://www.keil.com/mcb4300/mcb4300v1-3-schematics.pdf

-Dave @ NXP
0 件の賞賛
返信