EEPROM write endurance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM write endurance

ソリューションへジャンプ
2,096件の閲覧回数
vaclavrojik
Contributor II

Hello,

I have question about LPC11U24 on-chip EEPROM endurance. Value of parameter is per byte, or per 64B page?

When I wrote one byte to adress 0x0000, I shorted life for next 63 bytes in page, or not?

Thank You

Vaclav

ラベル(1)
0 件の賞賛
返信
1 解決策
1,900件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

When a single byte is programmed, the energy from the charge pump is concentrated on that one byte. If a page write is used, that energy is dissipated over more bytes, so cell wear is decreased.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,901件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

When a single byte is programmed, the energy from the charge pump is concentrated on that one byte. If a page write is used, that energy is dissipated over more bytes, so cell wear is decreased.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------