Deep sleep mode in LPC55S16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Deep sleep mode in LPC55S16

ソリューションへジャンプ
1,617件の閲覧回数
Balaji_KG
Contributor II

I need basic configuration to wake the controller from deep sleep mode on LPC 55S16. Any guidance?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,603件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, you have to select or design the waking-up source, which can wake-up the LPC55S16 from deep-sleep mode.

Pls refer to the section 14.4.5.3 Param2: wakeup_interrupts in UM11295.pdf

For example, if you select the WAKEUP_GPIO_INT0_0, you have to design a hardware button on the PCB.

If you select WAKEUP_CTIMER0, you do not require to do anything on the PCB.

From software,the deep-sleep waking-up follows up the interrupt process, for example, you use WAKEUP_GPIO_INT0_0, you have to configure the PINT0  and select the pin, so that the pressing the pin can trigger an interrupt.

 

xiangjun_rong_0-1684481123067.pngxiangjun_rong_0-1684481123067.png

Pls refer to the an13166.pdf and corresponding firmware.

https://www.nxp.com.cn/docs/en/application-note/AN13166.pdf

Hope it can help you

BR

XiangJun Rong

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,604件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, you have to select or design the waking-up source, which can wake-up the LPC55S16 from deep-sleep mode.

Pls refer to the section 14.4.5.3 Param2: wakeup_interrupts in UM11295.pdf

For example, if you select the WAKEUP_GPIO_INT0_0, you have to design a hardware button on the PCB.

If you select WAKEUP_CTIMER0, you do not require to do anything on the PCB.

From software,the deep-sleep waking-up follows up the interrupt process, for example, you use WAKEUP_GPIO_INT0_0, you have to configure the PINT0  and select the pin, so that the pressing the pin can trigger an interrupt.

 

xiangjun_rong_0-1684481123067.pngxiangjun_rong_0-1684481123067.png

Pls refer to the an13166.pdf and corresponding firmware.

https://www.nxp.com.cn/docs/en/application-note/AN13166.pdf

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信