Debugger probe problem LPC11U68

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger probe problem LPC11U68

2,906 Views
mohamedshaheen
Contributor I

I am using LPC11U68 eval board to program and debug a off board target processor (LPC11U68).

The debug session does not start and I get the following errors:

MCUXpresso IDE RedlinkMulti Driver v10.2 (Jul 25 2018 11:25:37 - crt_emu_cm_redlink build 555)
Reconnected to existing link server
Connecting to probe 1 core 0:0 (using server started externally) gave 'Ee(42). Could not connect to core.'
Connecting to probe 1 core 0:0 (using server started externally) gave 'Ee(42). Could not connect to core.'
Connecting to probe 1 core 0:0 (using server started externally) gave 'Ee(42). Could not connect to core.'
Server OK but no connection to probe 1 core 0:0 (after 3 attempts) - Ee(42). Could not connect to core.
Failed on connect: Ee(42). Could not connect to core.
No connection to chip's debug port

I saw similar postings but the suggested solutions did not work for me.

The debugger configuration is shown below:

Is there a known solution to this problem?

Thanks!

debugger config.JPG

Labels (1)
0 Kudos
Reply
4 Replies

2,659 Views
adamhimer
Contributor II

I am also having the Ee(42) issue on two different LPCXpresso V2 boards on a new PC build.

0 Kudos
Reply

2,659 Views
adamhimer
Contributor II

It seems my solution was disabling the enhanced peripheral service:
pastedImage_1.png

0 Kudos
Reply

2,659 Views
mohamedshaheen
Contributor I

Hi Adam,

Thanks the recommendation.  I unchecked "Use enhanced peripheral service" but it did not work for me.

I noticed that this error occurs when I power the target board from an external power source (not from the development board)

-Mohamed 

0 Kudos
Reply

2,659 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mohamed ,

Could you please take a picture to show how connect board?

Also please use the newest MCUXpresso IDE v10.3 to have a try.

BR

Alice

0 Kudos
Reply