Code Doesn't Run After Stopping Debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code Doesn't Run After Stopping Debug

跳至解决方案
1,926 次查看
caden013
Contributor III

Hi all, 

I have run into an issue with my LCP55S06-EVK board. While I have my board plugged up to my computer, I can build and debug my code, and my board runs the code perfectly. However, as soon as a stop the debug, my board stops running the code. It's as if if just gets stuck in the state in which it was when I stopped the debug. Also, upon unplugging my board from the computer and plugging it back in, the code does not run at all. 

This is a very frustrating problem, and I would appreciate any help.

Thanks in advance.

0 项奖励
回复
1 解答
1,918 次查看
converse
Senior Contributor V
2 回复数
1,919 次查看
converse
Senior Contributor V
1,913 次查看
caden013
Contributor III

Thanks for the solution! I had to use the NewLib (semihost).

0 项奖励
回复