Code Doesn't Run After Stopping Debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Doesn't Run After Stopping Debug

Jump to solution
1,928 Views
caden013
Contributor III

Hi all, 

I have run into an issue with my LCP55S06-EVK board. While I have my board plugged up to my computer, I can build and debug my code, and my board runs the code perfectly. However, as soon as a stop the debug, my board stops running the code. It's as if if just gets stuck in the state in which it was when I stopped the debug. Also, upon unplugging my board from the computer and plugging it back in, the code does not run at all. 

This is a very frustrating problem, and I would appreciate any help.

Thanks in advance.

0 Kudos
Reply
1 Solution
2 Replies
1,921 Views
converse
Senior Contributor V
1,915 Views
caden013
Contributor III

Thanks for the solution! I had to use the NewLib (semihost).

0 Kudos
Reply