Can CAN run on IRC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can CAN run on IRC?

1,052件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Tue Apr 21 10:02:10 MST 2015
Hello,

is it possible and is it a good idea to run CAN on IRC?
I assume IRC is not stable enough for CAN, but is this really the case?
Is there some document allowing or preventing this?

Best regards,

Martin
ラベル(1)
0 件の賞賛
返信
1 返信

1,044件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Apr 21 10:54:49 MST 2015

Quote: capiman
I assume IRC is not stable enough for CAN, but is this really the case?
Is there some document allowing or preventing this?



IRC is 1%, that's usually not a good idea  :((

See: http://www.can-cia.org/fileadmin/cia/files/icc/13/taralkar.pdf
0 件の賞賛
返信