Can CAN run on IRC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can CAN run on IRC?

1,074 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Tue Apr 21 10:02:10 MST 2015
Hello,

is it possible and is it a good idea to run CAN on IRC?
I assume IRC is not stable enough for CAN, but is this really the case?
Is there some document allowing or preventing this?

Best regards,

Martin
Labels (1)
0 Kudos
Reply
1 Reply

1,066 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Apr 21 10:54:49 MST 2015

Quote: capiman
I assume IRC is not stable enough for CAN, but is this really the case?
Is there some document allowing or preventing this?



IRC is 1%, that's usually not a good idea  :((

See: http://www.can-cia.org/fileadmin/cia/files/icc/13/taralkar.pdf
0 Kudos
Reply