CCAN with ROM functions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CCAN with ROM functions

1,175 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ipapp on Fri Nov 14 12:36:47 MST 2014
Hi,

Is there an example for the LPC43xx that uses the CCAN on-chip driver functions like there are examples for the LPC11xx(ie. this and this)? Or at least some documentation that explains how to implement it. There doesn't seem to be much information about this.

Thanks.
标签 (1)
0 项奖励
回复
1 回复

1,145 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Nov 14 13:36:45 MST 2014

Quote: ipapp
...for the LPC43xx that uses the CCAN on-chip driver...



:quest:

There's no CAN ROM API  :((

Chips with CAN ROM API are LPC11Cxx or LPC15xx...
0 项奖励
回复