CCAN with ROM functions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CCAN with ROM functions

1,169件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ipapp on Fri Nov 14 12:36:47 MST 2014
Hi,

Is there an example for the LPC43xx that uses the CCAN on-chip driver functions like there are examples for the LPC11xx(ie. this and this)? Or at least some documentation that explains how to implement it. There doesn't seem to be much information about this.

Thanks.
ラベル(1)
0 件の賞賛
返信
1 返信

1,139件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Nov 14 13:36:45 MST 2014

Quote: ipapp
...for the LPC43xx that uses the CCAN on-chip driver...



:quest:

There's no CAN ROM API  :((

Chips with CAN ROM API are LPC11Cxx or LPC15xx...
0 件の賞賛
返信