Battery Sizes for LPC8N04 Dev Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Battery Sizes for LPC8N04 Dev Board

1,860 Views
jameswhitney
Contributor II

Can't seem to find any specific information on the two different size batteries for powering the LPC8N04 Dev. Board.

Can someone give battery size/PN/voltages ?

Thanks,

J.

Labels (1)
0 Kudos
Reply
1 Reply

1,797 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi James,

This is the OM40002 design files, see if this can help you.

Board design files for LPC8N04 Revision B

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply