Battery Sizes for LPC8N04 Dev Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Battery Sizes for LPC8N04 Dev Board

1,928件の閲覧回数
jameswhitney
Contributor II

Can't seem to find any specific information on the two different size batteries for powering the LPC8N04 Dev. Board.

Can someone give battery size/PN/voltages ?

Thanks,

J.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,865件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi James,

This is the OM40002 design files, see if this can help you.

Board design files for LPC8N04 Revision B

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信