ADC VREFN in LPC5514JBD64E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC VREFN in LPC5514JBD64E

ソリューションへジャンプ
1,636件の閲覧回数
embedded_eng_
Contributor III

Hi,

I'm planning a PCB with the LPC5514JBD64E MCU.

The user manual specify that "VREFL is always from an external pin and must be at the same voltage potential as VSSA"  (39.4.1)

UM11295, https://www.mouser.com/pdfDocs/UM11295.pdf

 

 

On the other hand, the datasheet specify that VREFN is not connected to an external pin(64 pin HTQFP) (Table 3. Pin description)

https://www.nxp.com/docs/en/nxp/data-sheets/LPC55S1x_PDS.pdf

 

How can I use the ADC?

Does VREFN is internally connected to GND?

 

 

 

0 件の賞賛
返信
1 解決策
1,622件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  embedded_eng_

After confirm with internal,  VREFN is tied to VSSA internally.

 

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,623件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  embedded_eng_

After confirm with internal,  VREFN is tied to VSSA internally.

 

 

BR

Alice

0 件の賞賛
返信