ADC VREFN in LPC5514JBD64E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC VREFN in LPC5514JBD64E

Jump to solution
1,634 Views
embedded_eng_
Contributor III

Hi,

I'm planning a PCB with the LPC5514JBD64E MCU.

The user manual specify that "VREFL is always from an external pin and must be at the same voltage potential as VSSA"  (39.4.1)

UM11295, https://www.mouser.com/pdfDocs/UM11295.pdf

 

 

On the other hand, the datasheet specify that VREFN is not connected to an external pin(64 pin HTQFP) (Table 3. Pin description)

https://www.nxp.com/docs/en/nxp/data-sheets/LPC55S1x_PDS.pdf

 

How can I use the ADC?

Does VREFN is internally connected to GND?

 

 

 

0 Kudos
Reply
1 Solution
1,620 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  embedded_eng_

After confirm with internal,  VREFN is tied to VSSA internally.

 

 

BR

Alice

View solution in original post

0 Kudos
Reply
1 Reply
1,621 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  embedded_eng_

After confirm with internal,  VREFN is tied to VSSA internally.

 

 

BR

Alice

0 Kudos
Reply