2V Supply Voltage for LPC546xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2V Supply Voltage for LPC546xx

ソリューションへジャンプ
2,051件の閲覧回数
tiennguyen
Contributor I

Hi All,

This is the first time I use LPC546xx.

My system uses USB High-Speed then I have to use USB1. I must use 2V for VDD.

The question: Can I use 3.3V for USB1_AVDD3V3, USB1_AVDDTX3V3 and 2V for VDD, VDDA, VBAT, Vrefp?

If yes, is there any note that I must consider?

Thanks in advance!

ラベル(1)
1 解決策
1,976件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

For USB full-speed it is necessary VDD=3v min for operation while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V, for USB high-speed it is necessary VDD=1.71v min while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V.

Have a nice day!

Regards 

Soledad

元の投稿で解決策を見る

2 返答(返信)
1,977件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

For USB full-speed it is necessary VDD=3v min for operation while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V, for USB high-speed it is necessary VDD=1.71v min while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V.

Have a nice day!

Regards 

Soledad

1,976件の閲覧回数
tiennguyen
Contributor I

Hi Soledad,

Thanks for your confirmation.

Best Regards,

--

TN

0 件の賞賛
返信