2V Supply Voltage for LPC546xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2V Supply Voltage for LPC546xx

Jump to solution
2,057 Views
tiennguyen
Contributor I

Hi All,

This is the first time I use LPC546xx.

My system uses USB High-Speed then I have to use USB1. I must use 2V for VDD.

The question: Can I use 3.3V for USB1_AVDD3V3, USB1_AVDDTX3V3 and 2V for VDD, VDDA, VBAT, Vrefp?

If yes, is there any note that I must consider?

Thanks in advance!

Labels (1)
1 Solution
1,982 Views
soledad
NXP Employee
NXP Employee

Hi, 

For USB full-speed it is necessary VDD=3v min for operation while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V, for USB high-speed it is necessary VDD=1.71v min while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V.

Have a nice day!

Regards 

Soledad

View solution in original post

2 Replies
1,983 Views
soledad
NXP Employee
NXP Employee

Hi, 

For USB full-speed it is necessary VDD=3v min for operation while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V, for USB high-speed it is necessary VDD=1.71v min while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V.

Have a nice day!

Regards 

Soledad

1,982 Views
tiennguyen
Contributor I

Hi Soledad,

Thanks for your confirmation.

Best Regards,

--

TN

0 Kudos
Reply