2V Supply Voltage for LPC546xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

2V Supply Voltage for LPC546xx

跳至解决方案
2,076 次查看
tiennguyen
Contributor I

Hi All,

This is the first time I use LPC546xx.

My system uses USB High-Speed then I have to use USB1. I must use 2V for VDD.

The question: Can I use 3.3V for USB1_AVDD3V3, USB1_AVDDTX3V3 and 2V for VDD, VDDA, VBAT, Vrefp?

If yes, is there any note that I must consider?

Thanks in advance!

标签 (1)
1 解答
2,001 次查看
soledad
NXP Employee
NXP Employee

Hi, 

For USB full-speed it is necessary VDD=3v min for operation while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V, for USB high-speed it is necessary VDD=1.71v min while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V.

Have a nice day!

Regards 

Soledad

在原帖中查看解决方案

2 回复数
2,002 次查看
soledad
NXP Employee
NXP Employee

Hi, 

For USB full-speed it is necessary VDD=3v min for operation while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V, for USB high-speed it is necessary VDD=1.71v min while USB1_AVDD3V3 and USB1_AVDDTX3V3 are at 3.3V.

Have a nice day!

Regards 

Soledad

2,001 次查看
tiennguyen
Contributor I

Hi Soledad,

Thanks for your confirmation.

Best Regards,

--

TN

0 项奖励
回复