LPC微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC Microcontrollers Knowledge Base

讨论

排序依据:
Link to board: http://www.lpcware.com/content/devboard/android-open-accessory-aoa-kit Android Demos There are three demos available for download on the Embedded Artists website http://embeddedartists.com/products/app/aoa_kit.php The code bundle contains the following: Demo 1: Android Open Accessory demo which lets you control and monitor the AOA Board (LPC1769 side) from an Android device. Demo 2: Android Open Accessory demo which lets an Android device detect CAN nodes (such as the LPC11C24 side of the AOA board) in a CAN network. The CAN nodes can be controlled and monitored from the Android device. Demo 3: Android Open Accessory demo which lets an Android device detect Xbee nodes in an Xbee network. The Xbee nodes can be controlled and monitored from the Android device. FreeRTOS has been ported to the board and a demo is available that show how to use it. lwIP v1.4.0 has been ported to the board. The httpserver_raw (webserver) application from the lwIP contrib package is available with a small modification to use the on-board SD-card interface instead of the ROM based file system. FatFs file system module has been ported to the board. The lwIP demo (based on httpserver_raw) is using this module to access files on an SD card. nxpUSBlib is available and used in the AOA demos. How to setup the projects in LPC Xpresso Make sure that the latest version of the LPCXpresso IDE is installed. Download the package of sample application projects into the Eclipse workspace. The package can be downloaded (as a zip-file) from Embedded Artists’ support page after registering the product. The zip-file contains all project files and is a simple way to distribute complete Eclipse projects. Start the LPCXpresso IDE and select a new (and empty) workspace directory. Select the Import and Export tab in the Quickstart Panel and then Import archived projects (zip), see Figure 1 below. Browse and select the downloaded zip file containing the archived sample applications. Select all sub-projects to be imported, see Figure 2 below. By default the NXP USB library has been configured for USB device only. This needs to be changed to USB host. Right click on the nxpUSBlib project and select Build Configuration, then Set Active. In the list select LPC17xx_Host. See Figure 3. The projects are now imported. Click (to select) the project to work with. Click Build in the Quickstart Panel (under Start Here). See Figure 4 There is also a video on how to setup Demo 1 and get it running by connecting your android device. (Getting started video provided by Embedded Artists) http://www.youtube.com/watch?v=l3f2ss1IdV0&feature=player_embedded
查看全文
First, download the LPCXpresso54608 board User Manual.  After scanning the document, let's get started! Plug in LPCXpresso54608 (as shown below).  You will see the pre-loaded, Out of Box demo, which features Draupner TouchGFX.  A screen shot is shown below, Once you've explored the pre-loaded demo, you will likely want to learn more.   For this you will need to configure and build an MCUXpresso Software Development Kit (SDK) for your LPCXpresso54608 development board. Register or use your login credentials to sign in and download software from NXP. You can create a configuration for the LPCXpresso54608 in one of two ways: By typing 'LPCXpresso54608' or selecting boards>LPC>LPCXpresso54608 Once you have selected the board you will be presented with two options: 'Select Configuration' or 'Specify Additional Configuration Settings'. (It is recommended that you name the configuration something that specifies the settings as this will help identify multiple configurations.)   Note: By default the SDK Builder will choose IAR as the default toolchain for Windows.  For this tutorial we will use Windows as our Development Host OS.  If this is not the desired toolchain or OS please 'Select 'Specify Additional Configuration Settings' The following window will be presented, which allows you to download an SDK for IAR, Keil or Both (selecting 'All toolchains'.).  During this stage, you can also specify any necessary middleware for your download.  You can select or deselect these under the 'Select Optional Middleware' Select 'Go to SDK builder' once you have made your choices. Note:You may be prompted to update your info before you are allowed to download the package. If this happens select the link in the red at the top to resolve any issues. Once the information is updated you can click on the 'Overview' at the top and reselect 'SDK Builder' to return to the screen you were on. You have the opportunity to rename your file one last time before you hit download now. Once you select 'Download Now' you will be presented with a license agreement and once agreed to the download will start. Once you have downloaded the packaged .zip use your favorite utility to extract to a known location --> Continue here if IAR is your selected default toolchain. --> Continue here if KEIL is your selected default toolchain. --> Continue here if MCUXpresso is your selected default toolchain (coming March 2017!)
查看全文
Do you want to know more about one of our hottest products in the LPC800 series portfolio? Take a look at this technical presentation featuring the LPC84x MCU family. Based on the Arm Cortex-M0+ core, the LPC84x Family of MCUs is a low-cost, 32-bit MCU operating at frequencies of up to 30 MHz. The LPC84x MCU family supports of up to 64 KB of flash memory and 16 KB of SRAM. In addition, to make things easier, the LPC800 series McUs are supported by our free example code bundles and now, they're also supported by the MCUXpresso Software Develpment Kit (SDK).  Fig 1. LPC84x MCU Family Block Diagram
查看全文
LPC4088 Closed Payment Loop Demo - Compiling the software & flashing the board After connecting the three boards together, it's time to compile the software and flash it onto the board. To do so, please follow below steps. Download the software.​​ Unzip the software. Open the Keil Multi-Project workspace by opening the file .\LPC4088 POS Demo\Project_BlueboardPOS_Workspace.uvmpw. Note: Keil version V.4.54 or higher is required to open the workspace correctly. If you do not meet this requirement, an error will be shown when opening the workspace. Compile project "CDL" by right-clicking on the CDL project and selecting option "Set as Active Project" (1). Next, click on the "Rebuild" button (2) Repeat Step 4) for the 4 remaining projects (BSP, emWinlib, NxpRdLib_PublicRelease, Project_BlueboardPOS). Connect the Keil ULINK2 debugger to the baseboard (J8). If any other debugger than the Keil ULINK2 is used, the Keil project should be changed to use this other debugger. Power-up the board. Although the Embedded Artists base-board can be powered by a USB connection, it is advisable to use the power-jack because of the high-power consumption of the 7" LCD. Powering the board by USB may result in incorrect behavior. With project "Project_BlueboardPOS" set as active project, click on the "Load" button ( ). This will load the compiled POS demo to the FLASH. Proceed to "Running the demo"​
查看全文
Hello community!   Attached is a document that explains how to build and run the LPCOpen Ethernet example projects, it also explains the needed board and PC connections and configurations. The steps described in the document were done using the LPC1769 MCU like the one in the LPCXpresso board for LPC1769 with CMSIS DAP probe, but the same principles are applicable to any LPC MCU. The steps described in this document are valid for the following versions of the software tools: o    LPCXpresso v8.1.4 o    LPCOpen v2.xx Boards o    LPCXpresso board for LPC1769 with CMSIS DAP probe o    EA LPCXpresso BaseBoard o    LPC-Link2 Contents 1. Overview and concepts    1.1    LPCOpen       1.1.1 Core driver library       1.1.2 Middleware       1.1.3 Examples       1.1.4 LPCOpen with an RTOS 2. Running the lwip_tcpecho and webserver demo applications    2.1 Downloading a LPCOpen package    2.3 Setting up the hardware       2.3.1 LPCXpresso board for LPC1769 with CMSIS DAP probe       2.3.2 EA LPCXpresso BaseBoard    2.2 Importing the LPCOpen examples    2.4 Building the demo applications    2.5 Running the demo applications       2.5.1 lwip_tcpecho_sa demo       2.5.2 webserver demo Appendix A - References I hope you can benefit from this post, if you have questions please let me know.   Best Regards! Carlos Mendoza
查看全文
LPC China team creats a serial of LPC82x training slides with hands-on examples for GC customers, disti and fans. And all the material are written in Chinese. This is just the SCT chapter of the whole serials. Enjoy it. #sct‌ #lpc824‌ #lpc82x‌
查看全文
This content was originally contributed to lpcware.com by Jack Ganssle In this project I looked at the relative performance of the LPC4350's M4 vs. M0 cores, emulating ARM's big.LITTLE approach. In the last few years the industry has increasingly embraced the notion of using multiple processors, often in the form of multicore. Though symmetric multiprocessing – the use of two or more identical cores – has received a lot of media attention, many embedded systems are making use of heterogeneous cores. A recent example is ARM’s big.LITTLE approach, which is specifically targeted to smart phones. A big Cortex-A15 processor does the heavy lifting, but when computational demands are slight it goes to sleep and a more power-frugal A7 runs identical code. NXP’s LPC43xx also has two ARM cores: a capable Cortex-M4 and a smaller M0. Since power constraints are hardly novel to phones, my question was: “if we mirror the big.LITTLE philosophy, what is the difference in performance between the M4 and the M0?”
查看全文