simple GPIO interrupt example ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

simple GPIO interrupt example ?

5,416 次查看
johnbeale
Contributor II

I am using a Kinetis KL16Z128 processor, developing with KDS 3.0.0 and KSDK 1.2.0 / Processor Expert.  I am looking for a simple project code example of a GPIO input pin triggering an interrupt.  Is there one I can look at?  So far I have:

 

Component Inspector:

  gpio1:fsl_gpio    Input pin "SYNC_IN" Interrupt/DMA: Interrupt on falling edge

 

main.h: 

  extern volatile uint32_t syncCount;

 

main.c:

  syncCount = 0;  // count of sync line input signals (updated in interrupt routine)

  INT_SYS_EnableIRQ(PORTA_IRQn);

  INT_SYS_EnableIRQGlobal();

  do { various stuff... } while ( 1 );  // main loop

 

events.c:

  void PORTA_IRQHandler(void) {

    PORT_HAL_ClearPortIntFlag(PORTA_BASE);

    syncCount++;

  }

 

This compiles OK, and it runs, but I never see syncCount increment from 0, even though I am generating pulses on the PTA_4 input pin ("SYNC_IN") which I can detect using a normal port read from the main.c using  GPIO_DRV_ReadPinInput(SYNC_IN).

 

I have read through the document Interrupt handling with KSDK and Kinetis Design Studio  and it has useful information, but not quite enough for me to get a project working.  Any suggestions would be appreciated. Thank you!

标签 (1)
1 回复

2,580 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello John,

- Could you please show your code clearly , or how do you configure the component of fsl_gpio .

-  Under the SDK1.2 , there is a GPIO interrupt demo :

   Freescale\KSDK_1.2.0\examples\frdmkl26z\driver_examples\gpio

   this demo is about KL26, while the configuration is the same with KL16, you can refer to .

Hope it helps

Alice