frdm-kv31f PMSM ctrl with hall(an12374) code and pinmap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

frdm-kv31f PMSM ctrl with hall(an12374) code and pinmap

ソリューションへジャンプ
4,320件の閲覧回数
Frogram
Contributor I

Hi, all

I am looking "PMSM Field-Oriented Control on FRDMKV31F with Hall and Encoder Sensors(Doc No. AN12374)" now.

In that, "PMSM Package" appears. I followed them but I didn't get the same file or folder.

How and where can I get them? also, how can I check code and pinmap?

Thanks,.

0 件の賞賛
返信
1 解決策
4,314件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Frogram 

I hope that you are doing well!

The AN12374 comes with associated software that it needs to be installed in windows using an exe.  Please download and install >AN12374SW

If I understood properly your first question. In the path selected for the installation of the software , there are sub-folders corresponding to what the AN mentions as PMSM package structure.

diego_charles_0-1635310061910.pngdiego_charles_0-1635310061910.png

Regarding your second question about the  pin map. 

There is a file called pin_mux.c , where you can consult the pins that are initialized for the projects of the AN.

     diego_charles_1-1635310465740.pngdiego_charles_1-1635310465740.png

Note: To get the pin_mux file you will need to install the AN SW.

I hope this could help you. 

All the best,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,315件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Frogram 

I hope that you are doing well!

The AN12374 comes with associated software that it needs to be installed in windows using an exe.  Please download and install >AN12374SW

If I understood properly your first question. In the path selected for the installation of the software , there are sub-folders corresponding to what the AN mentions as PMSM package structure.

diego_charles_0-1635310061910.pngdiego_charles_0-1635310061910.png

Regarding your second question about the  pin map. 

There is a file called pin_mux.c , where you can consult the pins that are initialized for the projects of the AN.

     diego_charles_1-1635310465740.pngdiego_charles_1-1635310465740.png

Note: To get the pin_mux file you will need to install the AN SW.

I hope this could help you. 

All the best,

Diego.

0 件の賞賛
返信
4,305件の閲覧回数
Frogram
Contributor I

Thanks!
I have one more question, is that the freemaster is for only board SDK, not single processor?

0 件の賞賛
返信