frdm-kv31f PMSM ctrl with hall(an12374) code and pinmap

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

frdm-kv31f PMSM ctrl with hall(an12374) code and pinmap

跳至解决方案
4,350 次查看
Frogram
Contributor I

Hi, all

I am looking "PMSM Field-Oriented Control on FRDMKV31F with Hall and Encoder Sensors(Doc No. AN12374)" now.

In that, "PMSM Package" appears. I followed them but I didn't get the same file or folder.

How and where can I get them? also, how can I check code and pinmap?

Thanks,.

0 项奖励
回复
1 解答
4,344 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Frogram 

I hope that you are doing well!

The AN12374 comes with associated software that it needs to be installed in windows using an exe.  Please download and install >AN12374SW

If I understood properly your first question. In the path selected for the installation of the software , there are sub-folders corresponding to what the AN mentions as PMSM package structure.

diego_charles_0-1635310061910.png

Regarding your second question about the  pin map. 

There is a file called pin_mux.c , where you can consult the pins that are initialized for the projects of the AN.

     diego_charles_1-1635310465740.png

Note: To get the pin_mux file you will need to install the AN SW.

I hope this could help you. 

All the best,

Diego.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,345 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Frogram 

I hope that you are doing well!

The AN12374 comes with associated software that it needs to be installed in windows using an exe.  Please download and install >AN12374SW

If I understood properly your first question. In the path selected for the installation of the software , there are sub-folders corresponding to what the AN mentions as PMSM package structure.

diego_charles_0-1635310061910.png

Regarding your second question about the  pin map. 

There is a file called pin_mux.c , where you can consult the pins that are initialized for the projects of the AN.

     diego_charles_1-1635310465740.png

Note: To get the pin_mux file you will need to install the AN SW.

I hope this could help you. 

All the best,

Diego.

0 项奖励
回复
4,335 次查看
Frogram
Contributor I

Thanks!
I have one more question, is that the freemaster is for only board SDK, not single processor?

0 项奖励
回复