create kinetis SDK 2.x project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

create kinetis SDK 2.x project

4,178 Views
yiluxiangwan
Contributor II

I am a novice,I use KDS 1.3.

I want create kinetis SDK 2.x project , I don't know where this  SDK 2.0 root folder is .

Help.

Labels (1)
0 Kudos
Reply
5 Replies

3,201 Views
ivadorazinova
NXP Employee
NXP Employee

Hello.

Please can you specify your issue?

For downloading KSDK 2.0 is needed to use Welcome to Kinetis Expert | Kinetis Expert

Please take a look at following articles:

How to: install KSDK 2.0

Using Kinetis Design Studio v3.x with Kinetis SDK v2.0

I hope this helps you.

Best Regards,

Iva

3,201 Views
yiluxiangwan
Contributor II

Hi.

This is the case   :  Click  File>>New>>Kinetis SDK 2.x Project , Pop up a name is  Kinetis SDK 2.x project wizard   a window.      Select project name and SDK 2.x Path(root folder). 

My problem :   I don't know what SDK 2.x  path is .  I can't search the local document for information about it.

                         Can you tell me how to find the SDK 2.x  path?

Thank.

0 Kudos
Reply

3,201 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

The root folder is the folder you download , for example for the SDK_2.0_FRDM-K64F,

when you download it , it is a compressed files "SDK_2.0_FRDM-K64F.zip", please unzip it , when you create project,

the path is the folder "SDK_2.0_FRDM-K64F" (you can put this folder to anywhere ):

pastedImage_0.png

Hope it helps

Alice

3,201 Views
yiluxiangwan
Contributor II

I'm using K60.Nxp website is no K60 SDK 2.0,only have  SDK_1.3_TWR-K60D100M .  So,I cannot create about K60 kinetis SDK 2.x project.    

I think this is the case.

Thank you.

0 Kudos
Reply

3,201 Views
ivadorazinova
NXP Employee
NXP Employee

Hello,

yes exactly, because K60 is not supported by current KSDK 2.0.

But you can be calm, K60 will be supported in early of May.

I hope this helps you.

Best Regards,

Iva

0 Kudos
Reply