Windows 7 Driver for USB to SER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 7 Driver for USB to SER

2,694 Views
andrewsmit
Contributor I

We are using SDK2.0, on the K65F180. The USBSER driver works well in windows10 as the driver is automatically detected. In win7 I cannot get the virtual port detected. I have tested this on serveral machines, all WIN10 work, but not WIN7. I tried to copy the driver from WIN10 to WIN7, it is then detected, but does not work. Please help

(Window 10 automatically loads the driver and it works)

The USB info shows VID_15A2&PID_0300

0 Kudos
Reply
2 Replies

1,916 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Andrew

Please check the following post:

"MCU VIRTUAL COM DEMO" and demo app for USB-KW24D512 - can't find driver 

USB driver for VID_15A2&PID_0300 is located in the path <SDK_2.0_TWR-K65F180M_path>\boards\twrk65f180m\usb_examples\usb_device_cdc_vcom\inf, a file named fsl_ucwxp.inf

Hope this information could help you.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,916 Views
andrewsmit
Contributor I

Thank you, this worked

0 Kudos
Reply