Windows 7 Driver for USB to SER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows 7 Driver for USB to SER

2,645件の閲覧回数
andrewsmit
Contributor I

We are using SDK2.0, on the K65F180. The USBSER driver works well in windows10 as the driver is automatically detected. In win7 I cannot get the virtual port detected. I have tested this on serveral machines, all WIN10 work, but not WIN7. I tried to copy the driver from WIN10 to WIN7, it is then detected, but does not work. Please help

(Window 10 automatically loads the driver and it works)

The USB info shows VID_15A2&PID_0300

0 件の賞賛
返信
2 返答(返信)

1,867件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Andrew

Please check the following post:

"MCU VIRTUAL COM DEMO" and demo app for USB-KW24D512 - can't find driver 

USB driver for VID_15A2&PID_0300 is located in the path <SDK_2.0_TWR-K65F180M_path>\boards\twrk65f180m\usb_examples\usb_device_cdc_vcom\inf, a file named fsl_ucwxp.inf

Hope this information could help you.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,867件の閲覧回数
andrewsmit
Contributor I

Thank you, this worked

0 件の賞賛
返信