Why need to delay some time to get the correct data after check the LPUART_DRV_EdmaGetReceiveStatus?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why need to delay some time to get the correct data after check the LPUART_DRV_EdmaGetReceiveStatus?

1,160 次查看
hansonhe
NXP Employee
NXP Employee

Customer use K81, KSDK1.3 version, and have below question, 

Why need to delay some time to get the new data after check the LPUART_DRV_EdmaGetReceiveStatus?

 

Below is the question description:

LPUART_DRV_EdmaGetReceiveStatus(LPUART2_IDX, &uiCnt);

// We check uiCnt whether have new data,
// When UART have new data, we check from LPUART_DRV_EdmaGetReceiveStatus function, then read the DMA buffer data, the data is not latest data, we need to delay some time to get the buffer data after check the  LPUART_DRV_EdmaGetReceiveStatus function. If we delay 100us to read, we could got the latest correct data from s_aucRxBuf.

 

// Resource using is as below:
//1. LPUART2 receive use DMA function
//2. DMA BUF is 1024, it receive 200 bytes at one time


// DMA Init
int EdmaInit(void)
{
// Init eDMA modules.
edmaUserConfig.chnArbitration = kEDMAChnArbitrationRoundrobin;
edmaUserConfig.notHaltOnError = false;
EDMA_DRV_Init(&edmaState, &edmaUserConfig);
return 0;
}

// LPUART2 receive DMA init
int Lpuart2eDmaInit(void)
{
unsigned char uartchn;
lpuart_edma_user_config_t uartConfig;

uartConfig.clockSource = BOARD_LPUART_CLOCK_SOURCE;
uartConfig.baudRate = 115200;
uartConfig.bitCountPerChar = kLpuart8BitsPerChar;
uartConfig.parityMode = kLpuartParityDisabled;
uartConfig.stopBitCount = kLpuartOneStopBit;

LPUART_DRV_EdmaInit(LPUART2_IDX, &uartEdmaState, &uartConfig);

uartchn = LPUART2_IDX;
EDMA_DRV_InstallCallback(&uartEdmaState.edmaLpuartRx, Lpuart2EdmaRx_callback, &uartchn);
return 0;
}

 

// UART receive DMA config
void UartStartRecv(void)
{
LPUART_DRV_EdmaAbortReceivingData(LPUART2_IDX);
LPUART_DRV_EdmaReceiveData(LPUART2_IDX, s_aucRxBuf, 1024); // config buffer and size

}


void Lpuart2EdmaRx_callback(void *parameter, edma_chn_status_t status)
{
/* Stop DMA channel. */
EDMA_DRV_StopChannel(&lpuartEdmaState.edmaLpuartRx);

/* Signal the synchronous completion object. */
if (lpuartEdmaState.isRxBlocking)
{
OSA_SemaPost(&lpuartEdmaState.rxIrqSync);
}

/* Update the information of the module driver state */
lpuartEdmaState.isRxBusy = false;

UartStartRecv();
}

 

// UART receive function
u16 UartRxData(u8 *pDataBuf, u16 usLen)
{
u32 ulAvailLen = 0;
u32 ulBufWritePt;
unsigned int uiRC;
unsigned int uiCnt;
unsigned short usNowBufSaveLen;


LPUART_DRV_EdmaGetReceiveStatus(LPUART2_IDX, &uiCnt);

// We check uiCnt whether have new data
// If got the new data, we read the DMA buffer data, the data is not the latest data, we need to delay some time to get

// the buffer data. If we delay some time to read, such as 100us, we could got the correct data from s_aucRxBuf.


}

unsigned char Buf[1024];

void main()
{
EdmaInit();
configure_lpuart_pins(LPUART2_IDX); // LPUART2 pin init
Lpuart2eDmaInit();

while(1)
{
UartRxData(Buf, 256); //Why this interface function have delay when read data
}

标签 (1)
0 项奖励
回复
2 回复数

962 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Hanson He

Could you share the project from your customer, or at least the main.c file, I don't see where you start to receive data. I saw that you have:

void UartStartRecv(void)
{
LPUART_DRV_EdmaAbortReceivingData(LPUART2_IDX);
LPUART_DRV_EdmaReceiveData(LPUART2_IDX, s_aucRxBuf, 1024); // config buffer and size

}

but this function is inside the Lpuart2EdmaRx_callback, and this callback will be called when receive data register is full (this is set in LPUART_DRV_EdmaInit). So you aren't going to be able to received data until you call the function of receive data, and this is contradictory. I cannot prove this code in my side.

Waiting for your reply

Best Regards

Jorge Alcala

0 项奖励
回复

962 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Hanson He

Sorry for the late, How is your customer issue status? I'm working on this and I will inform you of anything that I find as soon as possible

Have a great day,
Jorge Alcala

0 项奖励
回复