Updated USB bootloader for K60?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Updated USB bootloader for K60?

1,479 Views
Deejay
Contributor III

Hi there,

 

I received an email re Kinetis Bootloader update but K60 is not included in the below list. Is there an updated USB bootloader for K60?

Thanks.

Regards,

Devan

62435_62435.pngpastedImage_0.png

Labels (1)
0 Kudos
Reply
1 Reply

1,323 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Devan,

The KBOOT V1.2 hasn't supported the K60, however you can port the exit bootloader demo to K60 by refer to KBOOT reference manual.

2015-08-11_11-21-48.jpg

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply