Updated USB bootloader for K60?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updated USB bootloader for K60?

1,557件の閲覧回数
Deejay
Contributor III

Hi there,

 

I received an email re Kinetis Bootloader update but K60 is not included in the below list. Is there an updated USB bootloader for K60?

Thanks.

Regards,

Devan

62435_62435.pngpastedImage_0.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,401件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Devan,

The KBOOT V1.2 hasn't supported the K60, however you can port the exit bootloader demo to K60 by refer to KBOOT reference manual.

2015-08-11_11-21-48.jpg

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信