Update fails for sdk 2.x project wizard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update fails for sdk 2.x project wizard

3,782 Views
stevescott
Contributor II

I cannot update KDS 3.2 to the new SDK 2.1 project wizard as per instructions in "Getting Started with Kinetis SDK (KSDK) v2.1" user guide, section 5.2.2:

 

170922_170922.pngpastedImage_1.png

 

170923_170923.pngpastedImage_2.png

Labels (1)
0 Kudos
Reply
8 Replies

3,606 Views
stevescott
Contributor II

Alice:

As I posted in my original message, I have KDS 3.2 which comes with the Kinetis SDK Project Wizard 2.0.0 already installed. I am trying to upgrade to the latest Project Wizard version.

This is what I have:

pastedImage_1.png

This is the latest version:

pastedImage_2.png

The version numbers are different. I have 2.0.0.201606291042. The latest version is 2.0.1.201610200920. When I "Check for Updates" Eclipse tells me there is a new version of the Project Wizard to install. But the upgrade is failing.

-steve

0 Kudos
Reply

3,606 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello steve,

The icon is grey,  it meaning the software has been installed .

And i think this has no effect on you developing your project .

While if you still want install it , please try first uninstall the former :

pastedImage_1.png

Then install the latest version as a mentioned .

BR

Alice

0 Kudos
Reply

3,606 Views
MarekTrmac
NXP Employee
NXP Employee

Steve,

if any update site does not work, you can disable it in main menu - Window - Preferences - Install/Update - Available Software Sites

Regards

Marek

0 Kudos
Reply

3,606 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello steve,

Please try to click Help ->Install New Software...

pastedImage_2.png

Then select "All Available Sites" , wait some minutes, it will show as below , then select the

"New Kinetis SDK 2.x Project Wizard", and install it:

pastedImage_1.png

Hope it helps

Alice

0 Kudos
Reply

3,606 Views
stevescott
Contributor II

Same error. It tries to update the previous version, but fails. I'm not doing a new install, just trying to update the existing version that came pre-installed in KDS 3.2 .

pastedImage_1.png

0 Kudos
Reply

3,606 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Steve,

Do you select the "--All Available Sites--" in the "Work With" ?

pastedImage_1.png

Please share the screenshots about your steps one by one , not only the error view .

Thus let me know when shows error .

BR

Alice

0 Kudos
Reply

3,606 Views
stevescott
Contributor II

I followed your instructions, just like you said.

The instructions you gave were for first time installation of the Wizard. When I followed your instructions, after clicking Next on the screen as shown in your previous post, Eclipse displayed a message that said the Wizard was already installed, and was switching to Update instead. Then it gave the same error message as before.

So neither method works - Check for Updates or Install New Software.

steve

0 Kudos
Reply

3,606 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Steve,

You said " Eclipse displayed a message that said the Wizard was already installed," .

So i think you have install it, please click the File -> New  to check whether have the KSDK2.x button :

pastedImage_1.png

I think yes,it have , you only need click it to develop your KSDKv2.1 project .

BE

ALice

0 Kudos
Reply