Upgrade from SDK v2.0 to SDK v2.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Upgrade from SDK v2.0 to SDK v2.1

1,300件の閲覧回数
Vagni
Contributor IV

I developed my project with KDS 3.2.0 and SDK v2.0.

Now, on my MCUXpresso area I was notified that my SDK library needed to be rebuilt, because the new SDK v2.1 was just released.

What is the better way to upgrade my project to the new SDK v2.1? Should I start with a new project and manually import all my source modules?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,167件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Hi Alessandro,

> Should I start with a new project and manually import all my source modules?

This is probably most easiest way.

Regards

Marek

0 件の賞賛
返信