Uninstalling Kinetis sdk 1.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Uninstalling Kinetis sdk 1.3

ソリューションへジャンプ
1,679件の閲覧回数
ronpeterson
Contributor I

I have installed the KSDK 1.3 but I need to remove it, it does not show up in the control panel and the installer does not have an option to remove it,   some guidance please

ラベル(1)
0 件の賞賛
返信
1 解決策
1,562件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The installer for the SDK 1.3 is basically a self-extracting zip file plus it sets an environment variable. So you simply can remove the inistallation folder from your disk. Check the system environment variables, it defines something like

KSDK_1_3_0_PATH=C:\NXP\KSDK_1.3.0

ointint to where you have installed it. Remove that variable too, and this should do it.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,563件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The installer for the SDK 1.3 is basically a self-extracting zip file plus it sets an environment variable. So you simply can remove the inistallation folder from your disk. Check the system environment variables, it defines something like

KSDK_1_3_0_PATH=C:\NXP\KSDK_1.3.0

ointint to where you have installed it. Remove that variable too, and this should do it.

I hope this helps,

Erich

0 件の賞賛
返信