Uninstalling Kinetis sdk 1.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uninstalling Kinetis sdk 1.3

Jump to solution
1,756 Views
ronpeterson
Contributor I

I have installed the KSDK 1.3 but I need to remove it, it does not show up in the control panel and the installer does not have an option to remove it,   some guidance please

Labels (1)
0 Kudos
Reply
1 Solution
1,639 Views
BlackNight
NXP Employee
NXP Employee

The installer for the SDK 1.3 is basically a self-extracting zip file plus it sets an environment variable. So you simply can remove the inistallation folder from your disk. Check the system environment variables, it defines something like

KSDK_1_3_0_PATH=C:\NXP\KSDK_1.3.0

ointint to where you have installed it. Remove that variable too, and this should do it.

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
1 Reply
1,639 Views
BlackNight
NXP Employee
NXP Employee

The installer for the SDK 1.3 is basically a self-extracting zip file plus it sets an environment variable. So you simply can remove the inistallation folder from your disk. Check the system environment variables, it defines something like

KSDK_1_3_0_PATH=C:\NXP\KSDK_1.3.0

ointint to where you have installed it. Remove that variable too, and this should do it.

I hope this helps,

Erich

0 Kudos
Reply