USB Simultaneous Host and Device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Simultaneous Host and Device?

ソリューションへジャンプ
2,348件の閲覧回数
randyhermes
Contributor III

Is it possible to run the USB stack in both host and device mode?

For example, I would like to have a Virtual Serial Port to talk to a PC and access a Mass storage device.

All the documentation I've seen discusses one or the other.

 

Thank You

Randy Hermes

ラベル(1)
0 件の賞賛
返信
1 解決策
2,238件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Randy,

Short answer is No you cannot do both host and device at same time.  It can be only one or the other.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,239件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Randy,

Short answer is No you cannot do both host and device at same time.  It can be only one or the other.

Regards,

David

0 件の賞賛
返信
2,238件の閲覧回数
randyhermes
Contributor III

Thanks David,

Randy

0 件の賞賛
返信