USB Simultaneous Host and Device?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB Simultaneous Host and Device?

跳至解决方案
2,471 次查看
randyhermes
Contributor III

Is it possible to run the USB stack in both host and device mode?

For example, I would like to have a Virtual Serial Port to talk to a PC and access a Mass storage device.

All the documentation I've seen discusses one or the other.

 

Thank You

Randy Hermes

标签 (1)
0 项奖励
回复
1 解答
2,361 次查看
DavidS
NXP Employee
NXP Employee

Hi Randy,

Short answer is No you cannot do both host and device at same time.  It can be only one or the other.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,362 次查看
DavidS
NXP Employee
NXP Employee

Hi Randy,

Short answer is No you cannot do both host and device at same time.  It can be only one or the other.

Regards,

David

0 项奖励
回复
2,361 次查看
randyhermes
Contributor III

Thanks David,

Randy

0 项奖励
回复