TWR-K65F180 UDP echo example: it doesn't work!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-K65F180 UDP echo example: it doesn't work!

跳至解决方案
6,227 次查看
mmoncigoli
Contributor III

Hello community,

 

I have big problems in communicating with my twrk65f180m board using UDP echo example present in KSDK_1.3.0 (it's the "lwip_udpecho_demo" example under "c\Freescale\KSDK_1.3.0\examples\twrk65f180m\demo_apps\lwip\lwip_udpecho_demo\...").

 

I am using MQX RTOS and KDS IDE (so I chose the proper UDP echo example under the path mentioned above).

 

PROBLEM DESCRIPTION

Sending a ping message from the PC, I cannot communicate with the twrk65f180m while it is running this example. The board is not receiving ANY data from the PC (I couldn't block the code with any breakpoint then).

 

MY PC CONFIGURATION

I sent a "ping 192.168.2.102" to the board from the Windows command console (as explained in "Kinetis SDK v.1.3 Demo Applications User's Guide.pdf"). I configured my PC with the fixed IP address = 192.168.2.101, Subnet mask = 255.255.255.0 and Default gateway = 192.168.2.100. I also tried to configured the PC with Default gateway = 192.168.2.101 (i.e. same of the IP address). Here attached you can find a screenshot of my LAN configuration. The software in the tower board is not giving any positive answer to the ping message

I tried to do the same thing with the ping example. Same result, no answer to a ping message.

 

 

Please, can anyone tell me how to make this example working on twrk65f180m?

 

Thanks so much for your

标签 (1)
1 解答
5,720 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi mmoncigoli,


Yes, it is different. Unfortunately we don´t have the driver DP83849, which is used on TWR-SER2. We have only driver for ksz8081 which is used on TWR-SER.

Kinetis does not have 2x 100Mb Ethernet PHY. TWR-SER2 is used mainly for Vybrid and ColdFire V52xx.

There is only one option - use TWR-SER, where the driver exists.

Best Regards,

Iva

在原帖中查看解决方案

0 项奖励
回复
7 回复数
5,720 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi mmoncigoli,

I tested on my side and the demo works without problems!

port.png

Please, be careful about jumper settings:

• Jumper J6 on position 1-2.

• Jumpers J1, J8, J10, J13, J14, J20, J24, J30 and J32 closed.

• Jumper J21, J19 all open.

• Jumpers closed on positions J22 (1-2, 3-4), J3 (1-2), J9 (5-6), J16 (1-2) and J27 (2-3).

• TWR-SER - CLK_SEL 3-4

• TWR-SER - CLKIN-SEL 2-3 (processor clock is taken from PHY)

• TWR-SER - ETH-CONFIG J12 9-10 to select RMII communication mode

• Important: Plug both the processor and the serial board (TWR-SER) into the Tower. The processor is using the

external clock from the Ethernet PHY on the serial card.

TWR-K65F180M system for Ethernet communication

Please let us know, if it helps you.

Best Regards,

Iva

0 项奖励
回复
5,720 次查看
mmoncigoli
Contributor III

Hello Iva,

Sorry about writing you again. Do you know if the reason of this weird/hard way to connect twrk65f180m board through this LWIP-UDP demo is due to using TWR-SER2 instead of TWR-SER, or if the reason is different?

For us it's important to know it, because a colleague of mine is using DHCP with this example, but he is not able to connect the board at all (neither following the unusual work-around I mentioned above).

Many thanks again

Regards

0 项奖励
回复
5,721 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi mmoncigoli,


Yes, it is different. Unfortunately we don´t have the driver DP83849, which is used on TWR-SER2. We have only driver for ksz8081 which is used on TWR-SER.

Kinetis does not have 2x 100Mb Ethernet PHY. TWR-SER2 is used mainly for Vybrid and ColdFire V52xx.

There is only one option - use TWR-SER, where the driver exists.

Best Regards,

Iva

0 项奖励
回复
5,720 次查看
mmoncigoli
Contributor III

Hello Iva,

Thanks a lot for your replies and investigation. At this point, I think, I can close this post as answered and get a TWR-SER board.

Many thanks again

5,720 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi mmoncigoli,

Sure, we will continue in a discussion because your issue is not solved.

With TWR-SER it works without problems. I apologize for my late response but I did not have TWR-SER2 for the testing.

Please give me short time to investigate this.

Thank you,

Have a nice day,

Iva

0 项奖励
回复
5,720 次查看
mmoncigoli
Contributor III

Iva, David,

First of all, many many thanks for your replies. I tried to run this demo with both openSDA (PEMicro) and JTAG (using SEGGER, so I used the DB-9 connector on the TWR-SER2 card), but with both failed. I checked all jumpers suggested by Iva and David. Everything ok on TWR-K65 (except J32, which I removed it just when I ran the test using JTAG with SEGGER). But I did NOT find the following jumpers on TWR-SER2 (they are supposed to be of TWR-SER, considering Iva's email):

• TWR-SER - CLK_SEL 3-4

• TWR-SER - CLKIN-SEL 2-3 (processor clock is taken from PHY)

• TWR-SER - ETH-CONFIG J12 9-10 to select RMII communication mode

In terms of PC configuration, please see the following picture (David, I can't leave gateway IP 0. You meant empty as in the pic here attached, correct?). I connected the TWR-SER2 directly to my PC. The latter, was once connected to the company's LAN and, during another test, just to the TWR-SER2.

PC Config.png

So, looking at David and Iva posts, I notice TWR-SER has been used, while I'm using TWR-SER2. Can this be the difference?

BUT I FOUND A "WEIRD" WORK-AROUND THAT MADE IT WORK!

But this is not supposed to be the right procedure provided by Freescale to run this demo. So, somewhere, there is something wrong. This is the procedure I followed in both released and debug modes:

a) Connect the ethernet cable to ETH port A of TWR-SER2 and run the demo. It does NOT reply to a "ping 192.168.2.102" command. I also tried lots of time to reset the board.

b) Connect the ethernet cable to ETH port B of TWR-SER2 and run the demo. It does NOT reply to a "ping 192.168.2.102" command. I also tried lots of time to reset the board.

c) Reconnect the ethernet cable to ETH port A of TWR-SER2 and run the demo. After different resets of the board (at the beginning it didn't work), it replies to a "ping 192.168.2.102" command. From now on it's working.

Any explanation about that?

Thanks so much for all your help, I really appreciate it.

0 项奖励
回复
5,720 次查看
mmoncigoli
Contributor III

By the way, I forgot to mention I'm using PE Micro with OpenSDA for debugging.

Thanks again to all will provide a help!

0 项奖励
回复