Size Project with Processor Expert Ciao

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Size Project with Processor Expert Ciao

1,378 次查看
vincenzogiudici
Contributor I

Ciao,

I created the project with processors Expert, but I realized that the dimensions are exaggerated ...almost 10K to configure only the micro KL03CSP without adding any driver !!

Oss then you can not implement?

How can I reduce the size?

Thank you

 

102035_102035.pngpastedImage_3.png

Original Attachment has been moved to: My_Project.zip

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,203 次查看
santiago_gonzal
NXP Employee
NXP Employee

Hello,

Processor Expert adds a lot of overhead. You can find attached a standalone project for KSDK 1.3 and KL03. You can create something similar using the KSDK Project Generator. It only uses 1Kb of Flash.

Regards,

Santiago

0 项奖励
回复