Size Project with Processor Expert Ciao

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Size Project with Processor Expert Ciao

1,387件の閲覧回数
vincenzogiudici
Contributor I

Ciao,

I created the project with processors Expert, but I realized that the dimensions are exaggerated ...almost 10K to configure only the micro KL03CSP without adding any driver !!

Oss then you can not implement?

How can I reduce the size?

Thank you

 

102035_102035.pngpastedImage_3.png

Original Attachment has been moved to: My_Project.zip

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,212件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello,

Processor Expert adds a lot of overhead. You can find attached a standalone project for KSDK 1.3 and KL03. You can create something similar using the KSDK Project Generator. It only uses 1Kb of Flash.

Regards,

Santiago

0 件の賞賛
返信