SDK support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDK support

跳至解决方案
4,460 次查看
pietrodicastri
Senior Contributor II

Good morning

I have problem in identifying the support of the SDK for the following processors:

 

MK10DN32VMP5

MK10DX32VMP5

MK10DN64VMP5

MK10DX64VMP5

MK10DN128VMP5

MK10DX128VMP5

 

Are any of supported???

 

Thank You

 

 

Pietro

标签 (1)
0 项奖励
回复
1 解答
4,267 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Pietro,

thank you for this very good question.

I checked your mentioned MCU and SDK support MCU and there is a main difference - there are different processors,

so there is no direct SDK support, but - I see support of KDS, so you can modify the code for KSDK.

I attach you the guide.

mk10.png

Does it help you?

Iva

在原帖中查看解决方案

4 回复数
4,268 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Pietro,

thank you for this very good question.

I checked your mentioned MCU and SDK support MCU and there is a main difference - there are different processors,

so there is no direct SDK support, but - I see support of KDS, so you can modify the code for KSDK.

I attach you the guide.

mk10.png

Does it help you?

Iva

4,267 次查看
EarlOrlando
Senior Contributor II

Dear Pietro,

I am afraid that there is only support for the Kinetis K10 that runs at 100 MHz (MK10DNxxxxxx10 and MK10DXxxxxxx10).

Regards,

Earl.

/* If this post answers your question please click the Correct Answer button. */

0 项奖励
回复
4,267 次查看
joetrovato
Contributor I

Similarly,

Is the Kinetis K70 at 120Mhz supported by the KSDK?

Thank you!

0 项奖励
回复
4,267 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Joe,

TWR-K70F120M will be supported in KSDK 1.3.

we expect it in Q3.

Best Regards,

Iva

0 项奖励
回复