SDK support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,649件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I have problem in identifying the support of the SDK for the following processors:

 

MK10DN32VMP5

MK10DX32VMP5

MK10DN64VMP5

MK10DX64VMP5

MK10DN128VMP5

MK10DX128VMP5

 

Are any of supported???

 

Thank You

 

 

Pietro

ラベル(1)
0 件の賞賛
返信
1 解決策
4,456件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Pietro,

thank you for this very good question.

I checked your mentioned MCU and SDK support MCU and there is a main difference - there are different processors,

so there is no direct SDK support, but - I see support of KDS, so you can modify the code for KSDK.

I attach you the guide.

mk10.png

Does it help you?

Iva

元の投稿で解決策を見る

4 返答(返信)
4,457件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Pietro,

thank you for this very good question.

I checked your mentioned MCU and SDK support MCU and there is a main difference - there are different processors,

so there is no direct SDK support, but - I see support of KDS, so you can modify the code for KSDK.

I attach you the guide.

mk10.png

Does it help you?

Iva

4,456件の閲覧回数
EarlOrlando
Senior Contributor II

Dear Pietro,

I am afraid that there is only support for the Kinetis K10 that runs at 100 MHz (MK10DNxxxxxx10 and MK10DXxxxxxx10).

Regards,

Earl.

/* If this post answers your question please click the Correct Answer button. */

0 件の賞賛
返信
4,456件の閲覧回数
joetrovato
Contributor I

Similarly,

Is the Kinetis K70 at 120Mhz supported by the KSDK?

Thank you!

0 件の賞賛
返信
4,456件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Joe,

TWR-K70F120M will be supported in KSDK 1.3.

we expect it in Q3.

Best Regards,

Iva

0 件の賞賛
返信