Run MQX 4.2 "Hello" Example on K66

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run MQX 4.2 "Hello" Example on K66

ソリューションへジャンプ
5,263件の閲覧回数
charles2
Contributor II

Hi,

I am trying to port the project to FRDMK66 with KDS 3.0 and MQX 4.2. I cloned the files from K65 and then made modifications on the linker and associated files referred to the porting guide and the porting examples. Right now, I have created MQX 4.2 library (including BSP and PSP), also successfully built and loaded the "hello" example (under MQX 4.2 example) to the board.

The problem is I cannot see the "Hello World" from the terminal (Tera Term) after loading the firmware or after resetting. Am I missing anything on the board file or any other files, like UART, USB etc.?

Any suggestions would be helpful. Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
5,156件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the differences between your board of the K66 and the K65. You need to check if there is not different UART peripheral or different pins.

Please refer to the porting guide attached.

I hope this helps, have a nice day!

Regards

Soledad

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
5,157件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the differences between your board of the K66 and the K65. You need to check if there is not different UART peripheral or different pins.

Please refer to the porting guide attached.

I hope this helps, have a nice day!

Regards

Soledad

 

0 件の賞賛
返信