Run MQX 4.2 "Hello" Example on K66

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run MQX 4.2 "Hello" Example on K66

Jump to solution
5,351 Views
charles2
Contributor II

Hi,

I am trying to port the project to FRDMK66 with KDS 3.0 and MQX 4.2. I cloned the files from K65 and then made modifications on the linker and associated files referred to the porting guide and the porting examples. Right now, I have created MQX 4.2 library (including BSP and PSP), also successfully built and loaded the "hello" example (under MQX 4.2 example) to the board.

The problem is I cannot see the "Hello World" from the terminal (Tera Term) after loading the firmware or after resetting. Am I missing anything on the board file or any other files, like UART, USB etc.?

Any suggestions would be helpful. Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
5,244 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the differences between your board of the K66 and the K65. You need to check if there is not different UART peripheral or different pins.

Please refer to the porting guide attached.

I hope this helps, have a nice day!

Regards

Soledad

 

View solution in original post

0 Kudos
Reply
1 Reply
5,245 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the differences between your board of the K66 and the K65. You need to check if there is not different UART peripheral or different pins.

Please refer to the porting guide attached.

I hope this helps, have a nice day!

Regards

Soledad

 

0 Kudos
Reply