I am working on FRDM-K64F board. I build the project and after debugging I get the following:
No source available for "(gdb[1].proc[42000].threadGroup[i1],gdb[1].proc[42000].OSthread[1]).thread[1].frame[0]"
No source available for "0x3848"
No source available for "0x2592"
The address keeps changing. I also get the following warning on the console:
Warning: the current language does not match this frame.
Temporary breakpoint 2, main () at ../Sources/main.c:65
65 PE_low_level_init();
Hi, Kiran,
Regarding your issue, we need to know the tools and version you are using, for example KDS/IAR/Keil...,if it is convenient, you'd better attach all your project so that we can have a debug.
BR
Xiangjun Rong
Hey kirantujare,
did you ever resolve this issue?
Thanks for your time,
Jason
Hi Jason,
Yes, it has been resolved.
Thank you,
Kiran Tujare