Makefsdata question!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Makefsdata question!

2,051 Views
jschepler
Contributor III

I recently ran the HTTP Server Demo on lwIP TCP/IP stack on an FRDM K64F.  It was a successful run.  I ran this Bare Metal (no RTOS).  Now I want to edit the webpage. Inside the fs folder are two very basic .html files that I created. However, when I run the Perl makefsdata, I get an error message of "FIND: Parameter format not correct."    Is there a way around this error? Also, if I install the MQX OS, does the httpserv demo use lwIP?

Tags (4)
0 Kudos
Reply
0 Replies