Lwip httpsrv demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lwip httpsrv demo

2,192件の閲覧回数
a8Chcx
Contributor V

Hi,

 

I am testing Lwip httpsrv demo project with KDS3.2 and KSDK 2.0 on FRDM-K66F. The demos(BM/RTOS) are working fine on Google Chrome... When I use IE8 on XP, it stop working. Even I can't ping after...

 

Is there anyone know the reason and workaround with IE?

 

Thanks,

 

Christie

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,799件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Christie,

This demo was tested on Win7.

I can confirm that the demo works on all browsers.

Unfortunately I don´t have any chance to test it under XP.

And what about another browser in XP? Did you try it in XP Chrome, Firefox, Opera? What was the result?

I apologize, but I don´t have the chance to test it in XP.

Have a great day.

Iva

0 件の賞賛
返信

1,799件の閲覧回数
a8Chcx
Contributor V

Hi Iva,

It works with Chrome on XP, but not with IE8. I think it is related to IE version.

Do you test with IE11 on Windows 7 and works?

I want to know which version this server is working on and let the customer to use the required browser?

Thanks,

Christie

0 件の賞賛
返信

1,799件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Christie,

Yes exactly. I can confirm it works on the newest browsers. These are required :

IE11, Win7.

Google Chrome 50, Win7

Mozilla Firefox 46, Win7

Opera 37, Win7

I hope this helps you.

Best Regards,

Iva

0 件の賞賛
返信