KV5X Clock configuration.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KV5X Clock configuration.

1,359 Views
arimendes
Contributor III

Hi,

I used the new Clock tool to do a new clock_config.c file for the KSDK 2.0 project in my MKV58 custom board.

The board use a external 16 MHZ crystal.

I want the CPU with 240MHZ, Fast peripheral clock at 120MHZ, flexbus at 60MHZ and flash at 24MHZ.

But when I test the board, the crystal don't oscilate and the code excution gets stuck at the Clock_SetExternalClkConfig function.

Someone could send me a clock_config.c file that works with my configuration?

 

Ari.

Labels (1)
0 Kudos
Reply
1 Reply

1,184 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

This post is going to be answered in this one: KV5x crystal, Clock and pins tools for desktop. 

Have a great day

Best Regards.

Jonathan

0 Kudos
Reply